(2)| 3/1/2017 10:34 AM | |
|
Joined: 4/28/2015 Last visit: 1/7/2026 Posts: 578 Rating:
|
Are you addressing https://bugs.debian.org/cgi-bin/bugreport.cgi?bug=738575? I'm also pretty sure that there are more applications affected by this, they just crash less frequently. That's the reason why we do not officially support a standard distro, nor does Intel. If you did it cleanly, you had to rebuild one from scratch, i.e. create your own port. |
| 3/2/2017 6:08 PM | |
|
Posts: 30 Rating:
|
I'd compile with the appropriate flags as they did with the Yocto image: -Wa,-momit-lock-prefix=yes |
| 3/2/2017 8:51 PM | |
|
Posts: 3 Rating:
|
Tanks for the hint. I didnot see this before. I will try and report here. |
| 3/28/2017 7:18 AM | |
|
Joined: 4/28/2015 Last visit: 1/7/2026 Posts: 578 Rating:
|
FWIW, just recalled a thread on LKML that pointed out two more applications breaking under Debian on Quark
It's clearly not recommendable to run Debian without very careful tests (some crashes can be less reliable due to the nature of the bug) or a complete rebuild on an Quark platform, including the IOT2000. |
Last edited by: jan-k at: 3/28/2017 7:20:20 AM |
|
| 5/9/2018 10:47 AM | |
|
Posts: 6 Rating:
|
Is it possible to install MYSQL server on this version? |
| 7/20/2018 8:13 AM | |
|
Posts: 18 Rating:
|
Hello Have you managed to install the MySQL server? |
Follow us on