(0)| 3/16/2017 1:25 PM | |
|
Posts: 1 Rating:
|
Hello, Every one I have some issue with function module FM354 . i am using fm 354 with steel shear dc motor . some times the shear doesn't cut , and this happens randomly, i want to make sure that the module outs th set point and the motor respond to it , this can be done online by using thr "trace" function in fm parameterization tool , one can plot set point velocity against actaual velocity , but you need to stay beside PG 24 hours , so i need to Plot historical trend of set point velocity against actual value velocity on scada , The problem is I can't find the memory adress that represents setpoint velocity and actual value velocity in the memory Mapping of the module.. thanks alot ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/17/2017 1:15:57 PMNew subject after splitting |
|
Follow us on