(1)| 4/10/2017 3:12 PM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12480 Rating:
|
Hello SOble; Without the dongle the Modbus RTU functions are not loaded to the CP 341. So it is essential that you purchase the dongle for this type of test, if you want to use the Siemens loadable driver for CP 341. Did you know that our friend TIBI68 has developped a Modbus master block for the CP 341 that does not require a dongle? It is completely independant of the Siemens driver, so you would have to study it and integrate it in your program, and there can be no Siemens support, although TIBI68 does give hints and solutions when a problem is detected. MODBUS RTU MASTER FOR CP340/341/441-X (NO DONGLE REQUIRED) Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
| 4/11/2017 10:04 AM | |
|
Posts: 511 Rating:
|
Hello Duris_I, and thx a lot for hetting involved in order to help me. I have two cubicles and inside each there are 2 CPUs s7-400H Inside third cubicle is S7-300. Inside fourth cubicle is ET200s, but fourth cubicle is 5 kilometres away from these 3 cubicle I mentioned before. SCADA is next to these 3 cubicles. SCada must communicate with 4 devices in some other cubicles which supports RTU RS485. On the end I have decided to place s7-1200 1212C (6ES7212-1AE40-0XB0) and CM 1241 RS422/485 6ES7241-1CH32-0XB0 into cubicle with with S7-300. S7-1200 with MODBUS collects data from 4 protection relays SEL-787 PUT/GET takes data to the S7-300 from S7-1200. Scada read data from S7-300 |
Last edited by: SOble at: 4/11/2017 10:06:23 AM |
|
| 10/10/2017 11:30 AM | |
|
Posts: 8171 Rating:
|
New question published by Willybong is split to a separate thread with the subject How many stations MODBUS RTU slave could I have?. Best regards |
Follow us on