5/9/2017 11:05 AM | |
Posts: 111 Rating: (1) |
I am using Win CC Runtime to display the messages on one big TV for everyone to see and identify where the problem is. I have too many machines and just displaying the name of the machine on the TV but if more than one machine goes down then I can only see one machine message on the TV. The problem is that any machine can go down anytime and it can be multiple machines go down at the same time. I want to have something so I can see all the messages on top of each other by flashing. If anyone have any idea then I will appreciate it also attaching the image as a reference. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/9/2017 12:08:49 PMNew subject after splitting Last edited by: Min_Moderator at: 5/9/2017 12:10:22 PMUpload attachment |
|
Follow us on