(0)| 6/7/2017 9:28 AM | |
|
Joined: 12/7/2009 Last visit: 11/12/2025 Posts: 33 Rating:
|
Hi, In view of Industry 4.0 revolution, of late we are facing a new requirement in which a data table need to be pushed directly into the SAP database from a S7-1200 station. SAP is currently an established enterprise software to manage business operations, the data analysis & presentation is managed by SAP server & it can have clients all around the globe. So the requirement is also seems to be very genuine that if there is a method to push the production data in almost real time into a dedicated structured table in the SAP database or an SQL database. Further integration with SQL database & SAP will be left to IT. Need to understand if this is possible to achieve from S7-1200 & if yes any sample application is available. Adding IEC or DNP3 modules to S7-1200 station is also allowed if possible. Thanks in advance. |
| 8/11/2017 2:14 PM | |
|
Posts: 8171 Rating:
|
New question published by klllll is split to a separate thread with the subject TRNASFER CSV FILE INTO SAP USING SOME .NET MODULE . Best regards |
Follow us on