9/4/2017 1:48 PM | |
Joined: 8/3/2009 Last visit: 8/7/2024 Posts: 13486 Rating:
|
Helo The *.fwc file ist the executed Runtime file of your Runtime Project. The *.pwx file is the File with User Administration informations. When the Runtime starts then the *.pwx file will be imported and the User Administration will generate one of the *.pwl files. If you use Recipes and datarecords for transfer then the data is in pdata.recipe.zip. This will be imported into the real recipe locatio nwhich you can define in the recipe engineering. The other files I do not now exactly their meanig. If you just want to backup your RT Advanced Project then store the complete folder in which the runtime file is (after loading into the RT PC). and if you use Recipes then backup also the folders you define in the Recipe properties in engineering. If you just want to now all necessary files for RT Transfer then use: https://support.industry.siemens.com/cs/de/en/view/109740696 (yes it works also with RT Advanced!) I think this should be enough information. Bye Murof |
Last edited by: Murof at: 9/4/2017 1:48:29 PMLast edited by: Murof at: 9/4/2017 1:50:42 PMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on