(0)| 9/21/2017 4:09 PM | |
|
Posts: 1 Rating:
|
hello, We want to replace an old PC that is connected to a Profibus network ( for an old WinCC system). Does a CP5711(USB conversion) offer the same options as a builtin CP5612 or 5622? In the near future there will be a revamp and the system will be converted to communicate through TCP/IP. So if a CP5711 can do all the things a build in module can do, we can remove it later. Kind regards, Lars ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/22/2017 8:59:31 AMNew subject after splitting |
|
| 9/22/2017 9:16 AM | |
|
Joined: 5/12/2006 Last visit: 1/14/2026 Posts: 22800 Rating:
|
Hello, yes this should be no problem. Regards Christoph |
Follow us on