(0)| 10/27/2017 1:05 AM | |
|
Posts: 5 Rating:
|
Dear All, I'm having an issue regarding Modbus TCP. I have a Sicam PAS that I have to communicate with Power Meters Siemens Sentron PAC4200 and PAC3200. Both type of devices are configured in the field to communicate with Modbus TCP protocol. (just IP address, subnet mask and gateway numbers) On the PAS Configuration, I'm not sure how to include them in my project, because if I add an aplication Modbus Master, the data requested to configure this type of application is interface (Type of protocol I selected Modbus TCP/IP) and then when I include the device I need to put IP address (I have this data) and the Modbus address (I don't have this, because the device communicates with Mobus TCP) I have only Modus Master license and I'm already communicating with other devices, but all of them have the IP address and modbus address (1...255). Could you please give me an advise on this matter? Do I need a different licence on my PAS? Best Regards, Marcos ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2017 1:09:27 PMNew subject after splitting Last edited by: marcsgonzalez at: 10/31/2017 6:19:00 PM |
|
Follow us on