(0)| 11/2/2017 9:41 PM | |
|
Posts: 1 Rating:
|
Hello guys, I have a Panasonic FP-X C14R PLC and i want to supervise it with WinCC runtime, is that possible? Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/3/2017 2:04:38 PMNew subject after splitting |
|
| 11/3/2017 2:54 PM | |
|
Joined: 9/27/2006 Last visit: 1/25/2026 Posts: 12482 Rating:
|
Hello Techniciens; Which version of WinCC are you using? WinCC v7,x? In that case you have an OPC channel in the WinCC conmmunications channels, as described in the following document: https://support.industry.siemens.com/cs/ww/de/view/102691766 As you can see in chapter 5 (especially section 5.4), through this channel WinCC can act as an OPC DA client. And with this optional software the Panasonic PLC can act as an OPC DA server: https://www.panasonic-electric-works.com/eu/plc-software-fp-opc-server.htm The Panasonic OPC server can communicate with the Panasonic PLC over Ethernet or serial connections, and since the PLC supports Modbus RTU (RS-485) you probably could set it up without an Ethernet module,. Call your Panasonic dealer to discuss this possibility. Hoper this helps, Daniel Chartier |
Last edited by: Jen_Moderator at: 11/6/2017 11:19:00 AMInserted right link. Last edited by: Jen_Moderator at: 11/13/2017 11:42:40 AMInserted right link. |
|
Follow us on