(0)| 11/23/2017 4:27 AM | |
|
Joined: 1/1/2014 Last visit: 7/30/2025 Posts: 1 Rating:
|
Dear Sir, Currently, i work with Siprotec with MLFB : 7SJ6221-4EB02-1FC0. As i found in setting serial port, it has 2 port: 1 PC port, 1 service port. I wonder that i read in catalog, the service port is port C, but my siprotec is installed in port B ( it should be system port) Now i need communication IEC-60780-5-103 protocol via system port. I want to ask that siprotec also accept service port in port B and it can change from service port to system port or not by download other firmware? P/S: my siprotec : Firmware V4.41.bootsystem: V01.03.03 Thanks so much. VungGV ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/23/2017 11:24:23 AMNew subject after splitting |
|
| 5/29/2018 10:55 AM | |
|
Posts: 8171 Rating:
|
New question published by Saituo is split to a separate thread with the subject Communication with 7SJ80 doesn't work: "unable to find correct catalog path. Geratyps does not exist...". Best regards |
Follow us on