(3)| 1/9/2018 7:28 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36467 Rating:
|
Something like this? You can set the following via the display: AttachmentRamp_over_weekly_timer_(0BA8.Standard).zip (361 Downloads) |
This contribution was helpful to
|
|
| 1/9/2018 7:42 PM | |
|
Posts: 8 Rating:
|
Yes, just like that. Thank you! |
| 1/9/2018 7:53 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36467 Rating:
|
You're welcome .... |
| 1/17/2018 9:01 AM | |
|
Posts: 5 Rating:
|
Hi: I modified the ixo65 program a little to fulfill with the requirement to do the ramping down at the set time. BR; Jaime AttachmentRamp_over_weekly_timer_(0BA8.Standard).zip (321 Downloads) |
This contribution was helpful to
|
|
| 12/31/2019 2:42 PM | |
|
Posts: 2 Rating:
|
Hi I can't open the file! do you know why? I am using Logosot Comfort V7 |
| 12/31/2019 2:57 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36467 Rating:
|
You wrote for thep roblem today also in another topic. You have not the right LSC version. You need LSC V8.0 or higher. Best is upgrading to the actually version 8.2.1, this upgrade is for free. You can download it from here: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) But it's a complete package with a size of 1,3 GB. After download start the Installation as an adminstrator. |
This contribution was helpful to
|
|
Follow us on