(2)| 1/20/2018 3:32 PM | |
|
Joined: 4/28/2015 Last visit: 7/14/2025 Posts: 58 Rating:
|
where is FB51 ?! I'm using pcs7 v9.0 but I can't find FB51 there 🤔 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/22/2018 10:37:49 AMNew subject after splitting |
|
| 1/20/2018 6:00 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Since PCS7 v8.x the default library is the AP library. FB51 is from the classic library before AP library was available. You have to install the PCS7 classic library from Additional Tools from the PCS7 DVD. The library is not updated anymore, no more support. The last version is V7.1 SP4. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 1/21/2018 2:35 PM | |
|
Joined: 4/28/2015 Last visit: 7/14/2025 Posts: 58 Rating:
|
Thanks ORECA, [snip] |
Last edited by: Jen_Moderator at: 1/22/2018 10:49:04 AMDivision of questions into separate topics. |
|
| 1/22/2018 10:47 AM | |
|
Posts: 8171 Rating:
|
New question published by 3 D J is split to a separate thread with the subject Is it possible to use FB51 in STEP5?. Best regards |
| 1/22/2018 12:46 PM | |
|
Joined: 10/26/2011 Last visit: 1/9/2026 Posts: 766 Rating:
|
Please note the additional comments to PCS 7 library. The PCS 7 library is still supported by the SIEMENS Technical Support. If you have problems with it or questions, you get support from the Technical Support. Also errors and defects will be solved with updates, see compatibility tool: What Oreca means, is that you will get no new features in the PCS 7 library. New features are only supported and developed with the Advanced Process Library (APL) or Add-On Libraries like Advanced Process Library (APG) or Industry Library (IL). Download - PCS 7 Library In the following entry, previous versions of the SIMATIC PCS 7 libraries supplied with the SIMATIC PCS 7 Software Media Package are offered for download (incl. PCS 7 Library V7.1 SP3 Upd4)
|
Last edited by: Thunderstorm at: 1/22/2018 12:47:24 PMLast edited by: Thunderstorm at: 1/22/2018 1:26:57 PMLast edited by: Thunderstorm at: 1/22/2018 2:16:23 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to
|
|
Follow us on