(0)| 3/15/2018 4:39 AM | |
|
Posts: 3 Rating:
|
Dear Experts, In Network 1 L P##DP_Address // Drive addressed mived is IW2500 LAR1 L 1 SLD 4 +AR1 L D [AR1,P#0.0] SRD 3 T #DRV_Add T MW 2130 In Network 2 L #DRV_Add T MW 2130 Above is part of function to Read/Write Drive Data, Where I pass Drive AddressIW2500 Can you explain me above program, I understand some part but not complete program what is use of L 1 SLD 4 And Why SRD 3 Also image is attached where I am seeing different values for same address, Network 1 MW2130 (Value, that is don,t understand) Network 2 MW2130 (2500) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/15/2018 2:41:31 PMNew subject after splitting |
|
Follow us on