(0)| 3/18/2018 4:29 PM | |
|
Posts: 179 Rating:
|
I have one question is it possible to use the Ethernet card on AK as OPC server ?? as far as I know SICAM AK maximum number of Ethernet card on two CPU and CP is 4 Ethernet using two SM2558 on CP 2017 and CPU 2014 . or I can increase the number of ports by adding CP 2017 to the main rack . what about if I have more than 50 devices which means 50 station on the AK ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/19/2018 6:43:19 AMNew subject after splitting |
|
| 3/19/2018 8:44 AM | |
|
Posts: 108 Rating:
|
SICAM AK doesn't support OPC protocol. |
Follow us on