4/1/2018 1:59 PM | ||||||||||
Posts: 19 Rating:
|
Dear Technical Experts. With reference to the previous discussion regarding existing library MODB4H does not support hot standby so we have procured new license (MODBUS TCP RED) with upgraded models as below:
1. How long it will take to get a license from Siemens once the request has been submitted as defined in procedure: https://support.industry.siemens.com/cs/ww/en/view/109739212 2. In chapter -5 of the same document, it is mentioned that "Note With an S7 H station only the CPU in rack 0 is licensed. For this reason, replacing the CPU from rack 0 after the licensing is no longer possible." In case, once I upgraded the 400H system with new model of MODBUS CPs, it means I will not be able to revert back?. Actually to be on safe side, since this modification involves the running plant so operation department always ask for backup / revert back plan. So how it will be possible to revert back to old condition (in case of any problem) once the new license will be moved to CPU / CP. ------------------------------------------------------------------------------------------ |
|||||||||
Last edited by: Jen_Moderator at: 4/3/2018 7:29:30 AMNew subject after splitting Last edited by: Jen_Moderator at: 4/3/2018 7:34:55 AMOptimized link. |
||||||||||
4/3/2018 7:31 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
New question published by WaqasKhalid is split to a separate thread with the subject How long it will take to get a license from Siemens?. Best regards |
4/4/2018 11:10 AM | |
Posts: 3093 Rating:
|
No, MODB4H works without registration key. |
This contribution was helpful to
1 thankful Users |
4/11/2018 9:52 AM | |
Posts: 3093 Rating:
|
yes |
Follow us on