6/5/2018 1:11 AM | |
Posts: 4 Rating: (1) |
Hello Siemens Forum I am trying to add an IP address to the switch.0001 interface of an RX1500. When I press the Commit button the unit displays a popup saying 'the configuration database is locked by session 49'. The new IP address is not added. Details of the unit as follows ... chassis model: RX1500 software loicense: Layer 3 Standard Edition Order-code: RX1500-L3-MNT-48-H1-L3SE-CG01-S01-6TX01-XX ROX Software Release: ROX 2.5.0 (2014-01-10) Thanks for your help. Regards Steve Hargraves (Australia) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/5/2018 7:14:14 AMNew subject after splitting |
|
6/5/2018 7:17 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice.
|
Follow us on