9/21/2018 8:57 PM | |
Joined: 9/1/2016 Last visit: 7/5/2024 Posts: 9 Rating:
|
OK After this network I had a reset from M2.3 to the same M2.3. Is it better to change the M?.? for a DB? Thanks |
9/21/2018 10:01 PM | |
Posts: 2826 Rating:
|
Tags within a DB is far less likely of being overlapped with each other. It is a bit more easy to stay organised. Tags from optimized DBs also process quicker - but don't be concerned about this point just yet. Asking you to use the tag was for two reasons: Notice also that you could have written your code inside an FB. The counter and all the other tags would then have originated from within the STAT parameter of the FB. ~ |
This contribution was helpful to
1 thankful Users |
Follow us on