10/26/2018 1:51 PM | |
Joined: 2/19/2016 Last visit: 8/4/2024 Posts: 19 Rating: (0) |
This entry shows you how to connect a PC station to an S7-1200 using OPC. A PC station and S7-1200 are configured together in a project in the TIA Portal https://support.industry.siemens.com/cs/gr/en/view/39960679 The first time i did it, it worked, i was able to monitor from OPC Scout V10 all my tags. Then from the moment i disconnect and and try again to connect, it didn't work again. The result of the variables are "Bad_waiting" I tried again the same procedure from the beginning with no result. i work in virtual machine, so i install from the beginning the simatic net V12 and follow the PDF, but never works. Please help me if you know something about this |
Follow us on