(0)| 7/8/2019 7:11 PM | |
|
Posts: 4 Rating:
|
I don't use a technological objects. Everything is done with move blocks. |
Last edited by: Jen_Moderator at: 07/09/2019 10:03:44Edited text for better reading. |
|
| 7/9/2019 7:01 AM | |
|
Joined: 4/28/2015 Last visit: 12/19/2025 Posts: 1278 Rating:
|
Hi, for the communication to the drive and for controlling it I would highly recommend to use one of those options: 1) use Technology Object 2) use the drive with standard telegram 1 and the Function Block "SINA_SPEED" from the DriveLib library, which is very simple to handle (just enabling the axis and giving a speed setpoint; as feedback you get the axis state and actual speed) - if Startdrive is installed to TIA you already have this lib installed, if not you can get it here: https://support.industry.siemens.com/cs/ww/en/view/109475044 |
|
Best regards, |
|
Follow us on