(0)| 9/21/2008 12:08 PM | |
|
Posts: 7 Rating:
|
Hello, How can I download STEP7 Version 5.4. I need CPU 414-2XK05-0AB0 GSD file. Thank you very much
|
| 9/21/2008 12:49 PM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12481 Rating:
|
Hello Siemens Users; Are you sure you want a gsd file for that CPU? Do you plan on inserting it as a Profibus-DP slave in a network? in that case, look at the following link, it providesa download for gsd files for Simatic CPUs: http://support.automation.siemens.com/WW/view/en/113652 Or do you need to see it in your Hardware catalog to be able toinsert it in your hardware configuration? If that is the case. what you need is a Hardware update. Depending on the version of Step 7 in your possession, you mayhave access to this function or not. But if this CPU is recent and its functionnalities are defined for Ste[p 7 v. 5.4 then either you will have to treat it as a lower version, or you will have to purchase the Step 7 v.5.4 upgrade. Look at the following thread, it is very recent and covers almost the same question: /tf/WW/en/Posts/21868#top Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/21/2008 1:12 PM |
|
| 9/21/2008 5:16 PM | |
|
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
Can youupload your hardware configuration here . Mean time you check http://support.automation.siemens.com/WW/view/en/2850229 /tf/WW/en/Posts/21868#top |
| 9/22/2008 2:11 PM | |
|
Posts: 487 Rating:
|
Hello, |
| 9/24/2008 3:31 PM | |
|
Joined: 11/30/2006 Last visit: 6/7/2024 Posts: 118 Rating:
|
To upgarde you need to buy Step 7 5.4 . Yes you definatly need Authoziration after Upgrading to Step7 5.4 . For more details on Installing and upgrading software check follwoing link , http://support.automation.siemens.com/WW/view/en/24834456 |
| 12/21/2015 3:40 PM | |
|
Posts: 4757 Rating:
|
New question published by siemensabbaco is split to a separate thread with the subject Load program to CPU 412 "HW missing". Best regards |
Follow us on