(0)| 4/17/2020 9:14 AM | |
|
Joined: 7/5/2017 Last visit: 12/12/2025 Posts: 6 Rating:
|
Hi, Yesterday I had a PLC going into stop, and the reason why is not clear for me. In the diagnostic buffer (in atachment) I found event 147 Maintenance demanded: Safety program: Warning limit cycle time exceeded Event ID: 16# 0D:75ED event 146 Error: PROFIsafe communication failure (timeout) Event ID: 16# 08:0318 event 145 Temporary CPU error: Maximum program cycle time exceeded Event ID: 16# 02:3501 What is the real cause of the CPU would it come from the safety or from the standard program? CPU is 1516F-3 PN/DP firmware V2.6.1 Kind regards, AttachmentDiagnostics1516F.txt (426 Downloads) |
| 4/20/2020 8:34 AM | |
|
Joined: 7/5/2017 Last visit: 12/12/2025 Posts: 6 Rating:
|
there are no loops programmed in the safety program |
Follow us on