(0)| 11/15/2008 7:17 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello About firmware SIMODRIVE 611 universal SIMODRIVE POSMO -SI, -CD, -CA Toolbox: Firmware and SimoCom U, Version 08.03 About where you can find firmware file, look at Manual(page 32) regards |
This contribution was helpful to
|
|
| 12/5/2008 5:23 PM | |
|
Posts: 271 Rating:
|
Hello Reid, Somehow you've decided that the firmware needs to be updated; however, you did not give the reason. Also, you did not say what version you currently have loaded. The firmware updates are located as a part of the Simodrive 611U Toolbox and there are many versions to choose from. Here is a link to the general download section: http://support.automation.siemens.com/WW/view/en/10804940/133100 The file type you need to download for firmware update is similar to the following: 611u_110206.zip ( 339 KB ) Once unzipped the file name will likely become 611u.ufw. I suggest that you use the latest SimoCom U (i.e., V11.2) and use the latest firmware, too, while you're at it. Hope this helps... |
| 12/25/2024 4:56 PM | |
|
Joined: 3/13/2015 Last visit: 9/22/2025 Posts: 1 Rating:
|
Hi, I need 611u firmware version V13.02.02 |
| 12/31/2024 8:10 PM | |
|
Joined: 10/17/2007 Last visit: 1/18/2026 Posts: 4579 Rating:
|
https://support.industry.siemens.com/cs/cn/en/view/45510964
|
Last edited by: Moderator_Lan at: 01/02/2025 08:27:54link optimized If you like my comments please |
|
Follow us on