(0)| 8/12/2020 1:01 PM | |
|
Posts: 1250 Rating:
|
You can assign only on interrupt *at one time* to CV=RV event but you can assign different hardware interrupt to the same event in the program, have a look here. It sounds like your encoder is two phase, how is it set up in the hardware configuration? You should be able to set both new count value and new reference value which I think you're saying they do work but not always. When you do a comparison do not use equal alone, use larger than or equal and less than or equal. Unloading the program would be a good idea, you can "archive" it the zip it and if it is not larger than 3 megabytes the it should upload. |
Follow us on