(2)| 9/25/2020 3:26 PM | |
|
Joined: 10/24/2011 Last visit: 12/12/2025 Posts: 4 Rating:
|
Hello everyone, I have a similar situation : no Profinet communication between PLC and robot. -robot Fanuc R-30iA -CP1604 v2.5, A05B-2500-J930 v2.5 mainboard A05B-2500-J930 -GSDML: GSDML-V2.25-Fanuc-J930-20120113.xml installed -PLC : S7-300 319F-3 PN/DP v3.2 -switch: SCALANCE X216 16 ports. The PING command to the IP of the robot works ,but the robot show up as offline in the online hardware config page. I am using Simatic Manager Step 7 V5.6 + SP2. Any thoughts on this? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2020 16:01:57New subject after splitting |
|
| 4/21/2021 7:31 AM | |
|
Posts: 1 Rating:
|
你好.我需要这个gsdml文件,方便给我一下吗?我们也有几台发那科R30iA的机器人,想试一下 |
| 4/23/2021 11:44 AM | |
|
Joined: 3/9/2018 Last visit: 8/21/2024 Posts: 5 Rating:
|
Dear, Is this an CP1604 card or an CP1616 card or a Molex card? |
| 10/31/2021 11:12 AM | |
|
Joined: 12/16/2020 Last visit: 11/4/2025 Posts: 2 Rating:
|
Did you got this gsdml? .. i am also searching for it. If possible with a example to use it in TIA. Thnx. |
Follow us on