(0)| 10/28/2020 4:00 PM | |
|
Joined: 2/6/2019 Last visit: 9/18/2024 Posts: 10 Rating:
|
I have the same problem. F7491 and F7492, EPOS stop cam reached. There is a reference to it here:https://support.industry.siemens.com/cs/ww/en/view/109481721 But even when i try the forced solution, (P29300=6), the same alarm keep coming. Its appears when the servo is in on state, and i start the reference mode to the encoder zero mark. I use an single turn absolute encoder. Anybody suggestions? EDIT: "When either of signals CWL and CCWL is not assigned to any DI, the signal will be at a high level automatically" ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_5218103 at: 10/28/2020 16:56:45Last edited by: Jen_Moderator at: 10/29/2020 07:55:34New subject after splitting. Optimized link |
|
Follow us on