11/16/2020 11:01 AM | |
Posts: 2 Rating:
|
Good Day, I am in need of information regarding CP341. I have a crane system consisting of four cranes communicating back to a storage warehouse manager via RS232 communications. The original system has 6es7 341-1AH01-0AE0 that communicates via Phoenix Contact RAD-2400-IFS- Wireless Transceiver. The above mentioned works and communicates with no issues, however the problem came in when the 6es7 341-1ah01-0ae0 had failed and a new one was purchased. The part 6es7 341-1ah01-0ae0 is now succeeded by 6es7 341-1ah02-0ae0. I then purchased the successor module and was advised that it is a direct replacement. I installed the module in the place of 6es7 341-1ah01-0ae0 and then commenced with power up. On power up the entire rack completes its start up as per normal, Plc module goes into run and RxD and TxD begin to flash as per normal, however the Warehouse storage manager indicates that the information coming back from this ''Crane''/"Module'' is unidentified. I then took a spare 6es7 341-1ah01-0ae0 from the adjacent crane, all four crane setup are fairly identical, and replaced the 6es7 341-1ah02-0ae0 with the adjacent 6es7 341-1ah01-0ae0 and boot up. Yet again everything boots up correctly, however this card works and the Warehouse manager receives information as per normal. system takes off and runs. could you please assist me with information or some remedy if possible. I am trying to understand what the difference are between the 6es7 341-1ah01-0ae0 and 6es7 341-1ah02-0ae0 are if the system goes into run in both instances with no error or system fault LED's. The setup in the 341 software is ASCII. speed is 1200bps. Data bits is 7. Stop bits is 2. Priority is Even. Please Team can you advise. If further information is required, please email me on [snip] Looking forward to hearing from you soon. Nirvaan Rambali. NirvzSA. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/16/2020 14:11:37New subject after splitting Last edited by: Jen_Moderator at: 11/16/2020 14:13:01Removed E-Mail address, doesn't comply with forum terms. |
|
Follow us on