(0)| 9/18/2021 1:20 PM | |
|
Posts: 15 Rating:
|
Hi there, Can upgrade windows 10 LTSB to LTSC after installing PCS7 v9.0 sp1 ? I have serious problem with Geforce GTX 1650 Ti driver .... afte 130 days i could not install and find 2015 driver for graphic card compatible with windows 10-2015 LTSB. please help me, i feel missouri. Tnx. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/20/2021 10:50:21New subject after splitting |
|
| 9/23/2021 9:09 AM | |
|
Joined: 1/11/2019 Last visit: 11/24/2025 Posts: 899 Rating:
|
Hi SINA400, It is not recommended to upgrade the OS from LTSB to LTSC. Siemens only provides recommendations and procedures with relevance to the PCS7 product line. PCS7 V9.0 SP1 on LTSC is not recommended by siemens. PCS 7 can only run-on operating systems that have been approved for PCS 7 (but Siemens does not recommend whether you could upgrade the OS or not - Before installing any PCS7 versions, it is important to ensure one of the recommended OS is installed). there could be possibilities of issues coming up with your proposed possibilities of OS upgrades which are not clear as yet. It is recommended by PCS7 to follow the guidelines for recommended Operating systems and IPC product line for a trouble-free upgrade experience. Please find the “3.3.1.2 Compatibility matrix SIMATIC IPC and accessories for PCS 7 V9.0 incl. SP1”in the attached file Hope this helps. Attachmentpcs7-readme_9.0 SP1.pdf (428 Downloads) |
Follow us on