(0)| 2/20/2009 11:04 AM | |
|
Posts: 34 Rating:
|
hi, thnx for the reply. i have no option to use a gear box. |
| 2/23/2009 11:36 PM | |
|
Posts: 271 Rating:
|
Hello MuthuLee, Not sure about true nature of your application; however, the 1FE1 series is excellent for this kind of thing. If you need a fully integrated package, the Weiss spindle division of Siemens is an excellent choice as well and they'll integrate the 1FE1 motors into their mechanical design. The motor you could consider is a 1FE1074-4WN11 which is rated for 41 kW from 7,000 to 20,000 rpm. It's rated torque is 56 Nm and at 10,000 rpm the toque is about 40 Nm for S1 duty. Go to www.automation.siemens.com/doconweb for the 1FE1 Configuration Manual. This motor can be driven by Simodrive 611U/D or Sinamics S120. Hope this helps... |
| 5/13/2016 12:33 PM | |
|
Posts: 4758 Rating:
|
New question published by Sarfraz Bhatti is split to a separate thread with the subject Alternative motor. Best regards |
Follow us on