(0)| 3/14/2022 8:14 PM | |
|
Posts: 1 Rating:
|
I to have this alarm today along with others. Machine ran fine on Thursday and was powered down as normal for the long weekend. started the machine today after the long weekend and it started up with errors. Error list on start up: 2001 - PLC has not started up 2101 - NCK battery alarm 2102 - NCK battery alarm 4060 - Standard machine data loaded 120202 - wait for connection to NC/PLC I replaced the battery with a new one this morning and restarted the machine. The following codes still appear. 2001 - PLC has not started up 120202 - wait for connection to NC/PLC Also during start up the machine says that Shop Mill fails to load and the machine screen opens in ISO. Never before has the machine started up on this side of the control previously. Please can some one point me in the direction to solving these issues, we have work to do. Tyson Labbe [snip] ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/15/2022 11:33:30New subject after splitting. Removed contact data, doesn't comply with forum terms. |
|
Follow us on