(1)| 2/17/2010 10:27 AM | |
|
Posts: 20 Rating:
|
r002=29.93 r003=220 r004=685 r005=25.6 r007=46 Measured value (with multimeter) = Phase to phase motor voltage=260V Phase to ground=246V |
| 2/17/2010 12:16 PM | |
|
Posts: 20 Rating:
|
ELIN motor typ:MKH-745 B06 FWB rpm:1030 6 pole torque:6490Nm |
| 2/18/2010 11:10 AM | |
|
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Hi Sorry for delay in reply.. I was little busy.. Now as per your data, At 30 Hz freq your torque is 6490*0.46 = 2985.4 Speed is 1030*30/60 = 515 -- I think your motor rated freq is 60 Hz Now for Power calculation, see attached document, P = M * n = 2985.4 * 515 = 154 KW I hope you are clear now.... Regards, Devesh Vithani AttachmentEquations - Formulaes.pdf (664 Downloads) |
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
|
|
| 2/18/2010 1:10 PM | |
|
Posts: 20 Rating:
|
Thanks your answer So, what about parameter of r005? You calculated power 154kW. How can we find 154kW using r005? best regards.. |
Follow us on