10/15/2010 10:47 PM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Dear ELSAVAN Yes , these functions are supported by PLCSIM V5.4 (here).But I personally believe that ,as I tested, just S7 connection with some SFB and FB can establish data exchange between to CPUs. 1-Please refere to here for list of usable functions. 2-Please refere here to see sample configuration, you can alter the project and use S7 connection with GET and PUT functions Best regards hdhosseini |
Last edited by: hdhosseini at: 10/16/2010 9:53 PM |
|
10/16/2010 8:15 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
<OFF TOPIC>
Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
10/16/2010 9:49 AM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Dear net experts Please check the following marked documment.SIEMENS claims that S7-PLCSIM supports some system functions which is listed in the attached documents.SFC14 and SFC15 are used to read and write data over PROFIBUS network.I personally think SIEMENS means these function can be executed in the simulator processor, no error will be generated (if config OK) but do not expect data exchange between 2 PLCs. Attachmentfunc=ll&o.zip (463 Downloads) |
This contribution was helpful to
1 thankful Users |
10/16/2010 10:04 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Yes, you are right. In my previous post for this reason put OFFTOPIC. My point was for ELSAVAN. What he is trying and how to use PLCSIM. Thank you and sorry for missunderstanding. Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on