(0)| 9/12/2011 2:08 PM | |
|
Posts: 3037 Rating:
|
Hello, You can migrate the OP20 to Protool with a convert tool.You can only migration the text.You need DOS knowledge. You get this tool of the Customer support.Then you can migrate this project to WinCCflexible. Tweety |
| 9/23/2011 10:45 AM | |
|
Joined: 7/5/2006 Last visit: 11/2/2025 Posts: 186 Rating:
|
thanks but how can i download the converter program? there is a link or something else ? have a good day
|
| 9/26/2011 8:19 AM | |
|
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, the OP20 is a real old panel. I also wouldn`t say "migrate" the panel, because everything you can migrate are the texts. So here are the steps you have to do to migrate the texts from a OP20 to a flexible panel: 1. convert the OP20 project with the software Konvert to ProTool How do you convert a COMTEXT project into a ProTool project? 2. migrate this ProTool project to flexible SIMATIC HMI WinCC flexible 2008 WinCC flexible 2008 Migration So if you have done all this and spend a lot of time you just get the texts from this old project. By the way, it is cheaper and faster to project a new project in flexible as using the old project. best regards |
| 4/11/2016 2:02 PM | |
|
Posts: 4757 Rating:
|
New question published by walter_g is split to a separate thread with the subject Where i can find the software COMTEXT?. Best regards |
Follow us on