(0)| 12/5/2006 12:47 PM | |
|
Posts: 48 Rating:
|
Hi everyone ! I wish to read data from a text file stored in the PCand display it on a MP277-panel. Is it possible ? thanks in advanced, Diogo |
| 12/8/2006 5:43 AM | |
|
Posts: 103 Rating:
|
I have done this with script on a TP270. I will forward the code when I next am available. |
| 12/8/2006 7:01 AM | |
|
Posts: 2348 Rating:
|
Sounds interesting for me too^) |
| 12/8/2006 8:40 AM | |
|
Posts: 317 Rating:
|
me too !![;)] Cheers |
| 12/9/2006 6:19 PM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi, I found a way to create a file on a PC. If you use the PC as a DNS server you can access from the panel to the shared folders of the PC. The IP address of the DNS server have to indicate in the network settings of the control panel. When you use the PC as a DNS server the name of the panel have to indicate in the host file of the PC. After that you can accesson the shared folders. Important: You can only access with the name of the computer - not with the IP address. I think this FAQ will help you: http://support.automation.siemens.com/WW/view/en/13336639 Bye |
| 4/10/2018 3:06 PM | |
|
Posts: 8171 Rating:
|
New question published by gauravhad00 is split to a separate thread with the subject How do create a new text file on button click using filectl object? . Best regards |
Follow us on