(0)| 11/6/2012 6:30 PM | |
|
Joined: 10/7/2005 Last visit: 1/21/2026 Posts: 3054 Rating:
|
Hello andreadbx you are correct, the cylic I/O related data can not exceed 244 Bytes as this limit universally applies to all DP Slaves. Your problem seems to be related tothe Parameter data though which are sent to each DP Slave on bus startup bythe DP Master as a once off. The limit for the Parameter data is also 244 Bytes if a GSD file based configuration is done. Typically though, you'd drag in the ET200S from the inbuilt HW catalogue (aka "metadata" based configuration) in which case Siemens employs a little DP-V1 related acyclic "trick" that allows you exceed the 244 Byte limit for theParameter data. There area few prerequsites for this to work though, which can be found on page 11 ofeachmanual for the IM151-1and which are: 6ES7151-1AA05-0AB0: For configurations as ofStep7 V5.4, it is possible to operate the IM151-1 STANDARD from 6ES7151-1AA05-0AB0 in DPV1 mode with more than 244 bytes of parameter data. |
Last edited by: fritz at: 11/6/2012 6:32 PMCheers |
|
| 11/7/2012 10:13 AM | |
|
Joined: 5/10/2011 Last visit: 1/15/2026 Posts: 20 Rating:
|
Thank you for your answer. My version of Step7 is v5.5 sp2 and every month I make hardware update so I think I have the last one. In effect I never try to change from DPV0 to DPV1. To solve the possible mistake about GSD file I download a new GSD folder here:https://support.automation.siemens.com/WW/llisapi.dll?query=im151-1+gsd&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=0&nodeid0=10805259 I try to make some test and then I report the result. |
|
Best regards |
|
This contribution was helpful to
|
|
| 8/17/2015 10:33 AM | |
|
Posts: 4757 Rating:
|
New question published by Razvansql is split to a separate thread with the subject IM151, can't see inputs and outputs. Best regards |
Follow us on