2/20/2013 1:21 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Try it with Updates of WinCC 7.0 SP3. After if the situation is the same -Support Request Best regards, Hristo Mihalev
|
This contribution was helpful to1 thankful Users |
2/21/2013 11:50 AM | |
Posts: 3 Rating: (0) |
@UMENCHO I try with updates, result is same. Thanks. @daga I try to add new channel but it doesn't allow another modbus. Actually i read 10 registers from each connection but the register address are not back to back. So i left one register for each driver connection result is same. I'm suspicious about Windows TCP-IP connection limit but i can't find any information about it. |
2/22/2013 11:27 AM | |
Posts: 1530 Rating: (59)
|
Hello yeux, that's a tricky situation, but you could try to ask Siemens Technical Support. Best regards Bizur |
This contribution was helpful to1 thankful Users |
11/19/2015 2:50 PM | |
Joined: 1/2/2014 Last visit: 3/12/2024 Posts: 142 Rating: (22) |
Any thoughts ? |
Follow us on