(0)| 3/26/2013 6:57 AM | |
|
Posts: 1525 Rating:
|
Yes, you can Connect 2 Wire Tx to 4 Wire Above mention Input Module Have alook on the Following Manual for the Connection In that Chapter 6.3 Figure no. 6-2 Point No 5 is the Configuration how you can connect it |
| 3/26/2013 7:44 AM | |
|
Posts: 62 Rating:
|
Yes, you can Connect 2 Wire Tx to 4 Wire Above mention Input Module Have alook on the Following Manual for the Connection In that Chapter 6.3 Figure no. 6-2 Point No 5 is the Configuration how you can connect it hello expert, the manual which you send is not match with the one which i send, once again i wish to conform it. |
| 3/26/2013 10:19 AM | |
|
Posts: 62 Rating:
|
dear sir, thank you so much |
| 10/8/2015 9:42 AM | |
|
Posts: 4757 Rating:
|
New question published by Marko80 is split to a separate thread with the subject How to connect to 6ES7134-4GB11-0AB0?. Best regards |
Follow us on