(0)| 10/11/2013 2:56 PM | |
|
Posts: 1368 Rating:
|
Hello, i don´t know S7-200 very well, but can it be, that you have to use another protocol? In the systemmanual of theS7-200 i found the following information As Client: max. 212 Bytes for XPUT/XGET As Server: max. 222 Bytes for XGET; max. 212 Bytes für XPUT and in Chapter 1.5.3 of this manual http://support.automation.siemens.com/WW/view/de/60590432/0/en?Datakey=24285698 Communications partners ● S7-200 CPU with CP 243-1 ● S7-300 CPU with CP 343-1, CP 343-1 Lean, CP 343-1 IT / Advanced ● S7-400 CPU with CP 443-1, CP 443-1 IT / Advanced ● PG/PC with OPC server ● PG/PC with STEP 7 Micro/WIN 32 The STEP 7 HW Config program shows you the types of S7-300 CPUs and S7-400 CPUs that support the S7 protocol XPUT/XGET and can therefore communicate with the CP 243-1. When you select an S7-300 or S7-400 CPU in the catalog of HW Config, this CPU must support the "S7 communication" function. I hope, i could help you. Pittiplatsch |
| 10/14/2013 6:45 AM | |
|
Posts: 20 Rating:
|
Hello! The following manual: https://support.automation.siemens.com/ww/llisapi.dll?func=cslib.csinfo&objId=23426892&load=treecontent&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW states that PUT/GET should work fine with S7-200 and S7-400. So I can't get why they don't work in full in my case... |
| 3/1/2018 6:49 AM | |
|
Posts: 8171 Rating:
|
New question published by ajrj is split to a separate thread with the subject Reference programm for communication with S7-200 (St60) and S7-300 over GET/PUT. Best regards |
Follow us on