5/25/2020 5:41 PM | |
Joined: 10/13/2017 Last visit: 1/13/2022 Posts: 20 Rating: (3) |
Hi, In the Full client you have to option to use the matrix object. In this matrix you can paste the counter values directly from a file (e.g. TXT, EXCEL, CSV). To create a new matrix you have to create data points at first. Please make sure that these data points have the categorty "Count value". Then you have to create the matrix object in the Full Client. You can find this object in the Acquisition tab. After hitting the Matrix Icon you have to select the 15 min cycle time in the matrix. As a query type you should select "Month". So, you should import the values for the 3 tags per month in order to avoid too high load on the matrix. Finally, you have paste the 3 tags underneath the matrix. By double clicking on the Matrix you can open the matrix. |
This contribution was helpful to1 thankful Users |
Follow us on