12/10/2014 12:39 PM | |
Posts: 11 Rating: (0) |
hii Thank for your suggestion george, we are doing projects for Pharmaceuticals industry. I'm handling it for the first time. please clarify my folowing doubts. 1. Is Audit trial is a separate software or it is integrated in Wincc SCADA 7.3 itself? 2. How to configure a audit trial viewer? 3. How to link the Wincc tags in it? If any Audit trial viewer backup link, please send it. ------------------------ New subject after splitting from Report generation with compliance of 21 CFR |
Last edited by: Min_Moderator at: 12/10/2014 5:09 PMSplitted |
|
12/10/2014 1:05 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello SARAVANAN MADHAVAN to your questions: 1. Is Audit trial is a separate software or it is integrated in Wincc SCADA 7.3 itself? --> Audit is an additional option for WinCC, see http://w3.siemens.com/mcms/human-machine-interface/en/visualization-software/scada/wincc-options/wincc-audit/Pages/Default.aspx 2. How to configure a audit trial viewer? The Audit Viewer is an additional application, which can be used without license. It displays the data from theAudit-Trail-database. 3. How to link the Wincc tags in it? You do not link tags. Changes made by operatores can be watched. For example:i You have a picture in WinCC-runtime with an i/O-field in it. To the I/O-field is a tag connected. If the operator changes the value in the i/O-field (tag), a operator-message will be generated. This operator-message will be transfered to the Audit-Trail-database. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on