7/8/2020 9:41 AM | |
Joined: 7/2/2020 Last visit: 2/28/2023 Posts: 14 Rating: (0) |
how do i enter in nc? and by the way the nc led in the left of the control, its flashing no matter if i am in mda, auto, jog or teach mode. Below i atach a small video.
Attachmentvideo-1594193802.avi (468 Downloads) |
Last edited by: corasalin at: 07/08/2020 09:43:15 |
|
7/8/2020 10:21 AM | |
Joined: 7/2/2020 Last visit: 2/28/2023 Posts: 14 Rating: (0) |
somehow i managed to enter NC/PLC variab. and i think its weird there. |
7/10/2020 8:17 AM | |
Joined: 7/2/2020 Last visit: 2/28/2023 Posts: 14 Rating: (0) |
hello, i meant if there is a M code to put it in MDA to reset magazine to 0, i have no tools in magazine, no tools in preloader, so maybe there is a M code to tell the machine that everythink is empty. The problem is that i don t have any backup of nc data. Preloader loads corectly the tools with the coresponding pocket that i set, but somehow it always tryes to put the tools to location 0002, even if i disable that location, so if i do N20 T=''T5'', N30 M6, then the magazine roates to pocket 5, the POT goes down and this is it, the error says that tool T5 cannot be putet on location 0002, invalid definition of magazine. It doesn't have sense, from my opinion. When the error come L13 led is flashing in electrical panel, i put a small video of that. Anyway i dont think i will solve this.
Attachmentvideo-1594361258.avi (440 Downloads) |
Follow us on