6/29/2010 12:42 PM | |
Posts: 5 Rating:
|
Hi all, I have another question over here. is the USB Prommer 6ES7 792-0AA00-0XA0 compatible with Simatic S5Version 7.21. Do you have any procedurce to burn the Flash card using USB Prommer + Simatic S5? My Flash Card is 6ES5 374-2FH21/ 6ES5 374-2KH21 thanks... rgds, CK Cheng Splitted from each time i want to install the software it will always 'Pop out" an error whick ask me to restart the Windows . |
Last edited by: O_Moderator at: 6/30/2010 11:00 AMnew subject after splitting |
|
6/29/2010 1:36 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, The program S5EPROM.EXE allows S5EPROM / EEPROM modules and S5 memory cards to be programmed using the SIMATIC USB-PROMMER. With this program, you can transfer, compare and read blocks from an S5 program file (*ST.S5D file) onto SIMATIC S5 modules. Transferring data from a file onto a memory module is also described as “load” with STEP 5. More info at SIMATIC S5 S5EPROM for USB prommer. Best regards, Hristo Mihalev |
6/30/2010 12:06 PM | |
Posts: 5 Rating:
|
Thanks a lot... I got it! |
This contribution was helpful to
1 thankful Users |
Follow us on