(0)| 3/11/2007 5:28 AM | |
|
Posts: 13 Rating:
|
We are having a S5 system with 6ES5 IM-308-6UA12connected toET100U system as described in the attachment.Whileburning the EPROM withtheCOM ET100, it terminates with an error message relating to the submodule. Please confirm the version of COM package required and any other point missed out by us. AttachmentANNEXURE 1.zip (1014 Downloads) |
| 3/11/2007 11:54 AM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, You can find the COM-packages with the different WINDOWS versions on Internet after the next link: Executability of COM Packages Under STEP 5/ST V7.1x Please also consider that the EPROM you are using is from a newer type, blowing this with old software will destroy the EPROM, I think you have to use COM EPROM or the newest COM ET100U I think that the card is a -3UA12, a -6UA12 I have never seen before, the configuration must be no problem. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
| 4/1/2007 4:41 PM | |
|
Posts: 13 Rating:
|
We are having a 6ES5 308-3UA12 IM to be linked with an ET100U station. After configuring the program, we tried to burn the EPROM (6ES5 376-1AA11) using COM ET 100 V2.1 software package on Step5/ST Version 7.2. It gives following error when "Blow EPROM" command is executed: "Faulty modulehandling !" However, each time the EPROM is erased, it does display empty while executing "Read EPROM" command. Therefore, i think the EPROM is OK. Attached is the configuration file (PENDENT1.308) for your info. Please suggest us a remedy. AttachmentErr_EPROM_01.zip (895 Downloads) |
| 4/3/2007 9:08 AM | |
|
Posts: 13 Rating:
|
I'm having Windows 98 OS, butstill boot it in MS-DOS mode while working with Step5. |
Follow us on