3/17/2006 12:51 PM | |
Posts: 5822 Rating: (412) |
Hello, J_Bell. |
4/10/2006 2:54 PM | |
Posts: 17 Rating: (0) |
ms win 2000 5.00.2195 sp4 |
5/21/2006 10:00 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi Harp, There is also a V5.3 SP3 HF1 and V5.4 of STEP7 is also available. Maybe that brings something [:(] If there is something in the registry that blocks another version some way then it never will work again, so what i have done sometime is deinstall all STEP7 packages and then use the FAQ http://support.automation.siemens.com/WW/view/en/189025where is described how to clear all data and the registry. It is some work but all dead bodys are gone after that! [:P] Then you start new and the hole registry is cleared about STEP7 and the packages. |
Last edited by: Late at: 5/21/2006 10:07 PMExtra information I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on