6/9/2020 1:02 PM | |
Posts: 1 Rating: (0) |
dear sir can you explain whats mean memory compressing and what the advantage disadvantage on it pls need manual to full understand it best wish thanks . ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/09/2020 13:11:27New subject after splitting |
|
6/24/2020 7:16 AM | |
Joined: 12/10/2018 Last visit: 6/27/2024 Posts: 109 Rating: (11) |
Hello dear muntadhersefaa This text is related to the opinions of a number of users regarding the issue, which will be shared with the relevant link. Supposedly in the new SIEMENS PLC, this process is automatic, although not always is working … anyway, if you did it manually and it is not compressing, it means you are actually using all this load memory …then it means that if you try to load some object bigger that 7kb (100-88)%, you are not going to have enough memory. I shouldn’t say that, but using VIPA what is the same than SIEMENS ( I have my doubts) I had a problem compressing, then I did a reset of the PLC, I reload the hardware configuration and it was working again … although not always is possible to do a total Reset. |
Follow us on