3/19/2021 9:30 AM | |
Joined: 1/12/2011 Last visit: 9/10/2024 Posts: 59 Rating: (5) |
Is there never a need for iw600:p with a S7-1200 CPU? |
3/19/2021 9:31 AM | |
Joined: 5/12/2006 Last visit: 9/25/2024 Posts: 22372 Rating: (3014) |
correct, no need. |
This contribution was helpful to1 thankful Users |
3/19/2021 9:39 AM | |
Joined: 1/12/2011 Last visit: 9/10/2024 Posts: 59 Rating: (5) |
OK, tnx for your quick reply. gr. |
3/22/2021 9:31 AM | |
Joined: 1/12/2011 Last visit: 9/10/2024 Posts: 59 Rating: (5) |
99.99% of the time normal cyclustime is OK and fast enough. Tnx. |
Follow us on