10/24/2021 12:45 PM | |
Joined: 9/27/2006 Last visit: 5/13/2024 Posts: 12257 Rating: (2668)
|
Hello engineer; This is how memory compression is explained in the Programming with Step 7 manual: https://support.industry.siemens.com/cs/ww/en/view/109751825 So there should be no effect on the programmed functions in the PLC. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
10/28/2021 8:16 PM | |
Joined: 1/4/2019 Last visit: 12/4/2023 Posts: 60 Rating: (0) |
thanks alot i made the compression of memory and it was successful . now the memory drops from 91% to be 28 % |
Follow us on