2/16/2010 8:24 AM | |
Posts: 7 Rating: (0) |
I have a PLC with a Tiway card that I am not sure is still used by the configuration. Am I going to have to track down the TIUSER/TIPROG software to investigate this card?
AttachmentENERGY RECOVERY 20091110c.zip (709 Downloads) |
2/16/2010 4:32 PM | |
Posts: 510 Rating: (117)
|
The file you posted is for Softshop. Here is a link to download Softshop if you can't find yours. http://www.sea.siemens.com/us/products/automation/programmable-controllers/Pages/programmable-controllers-simatic-505-downloads.aspx SoftShop requires a dongle to run. If you can't find the dongle, SoftShop will run in demo mode to view the program. But you won't be able to save changes or download to the PLC. The TIWAY PC board was ISA form factor. So unless you have some old PCs with ISA bus,the PLCmay not be connected toanything. You could use TISoft to make the hardware changes. I posted a copy in the forum. It is DOS based. billwest |
Follow us on