3/14/2011 5:44 PM | |
Posts: 4 Rating: (0) |
I'm facing a strange problem with a micro-automation project done in Siemens S7-1200 PLC. The small program I wrote compiles perfectly, and downloads successfully. But the CPU does not go into RUN mode. Diagnostics buffer shows "New startup inhibit information - Current CPU operating state: STOP". Also reports, "Pending startup inhibit(s): - HW configuration inconsistent (TIA portal activity) - Manual warm start required." I did the HW configuration alright, I know. Diagnostics status shows "The loaded configuration and the offline project are not identical. The online and offline module configuration data are different. Order number: 6ES7 214-1AE30-0XB0 Configured order number: 6ES7 214-1AE30-0XB0" The reported numbers are exactly same, I can't see why it's saying that the configurations are different. I tried to press the "RUN" button in online panel, I saw network activity in the CPU (Rx/Tx LEDs), RUN/STOP, Error, Maint LEDs blink. But the CPU does not start and repeats the above messages in diagnostics. I tried memory reset (MRES in online panel) also. Same result. I also tried to download a new project. That also behaved in this way. Most importantly, I changed the CPU, and the new CPU also did this same thing, which surprised me very, very much. Anyone experienced similar behavior? All helps are appreciated. Regards Rahul |
This contribution was helpful to1 thankful Users |
3/17/2011 3:38 PM | |
Joined: 7/7/2010 Last visit: 4/23/2024 Posts: 14615 Rating: (2348) |
Glad you got it loaded and running! |
science guy |
|
4/11/2022 11:03 AM | |
Joined: 3/23/2022 Last visit: 4/11/2022 Posts: 1 Rating: (0) |
thanks tom I did what you said and the problem was solved. |
9/30/2022 12:44 PM | |
Joined: 6/14/2022 Last visit: 1/30/2023 Posts: 1 Rating: (0) |
Thanks! I had the same issue and solved it this way. |
Follow us on