3/15/2012 5:18 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello RichardSapp, You do not need TIA Portal (STEP 7 v11) installed in order to access your Web Server of S7-1200 CPU. For more details on Accessing the Standard Web pages from PC. and Web server in S7-1200 from here. |
Like it? Rate it! |
|
3/15/2012 5:44 PM | |
Joined: 5/4/2009 Last visit: 4/30/2024 Posts: 914 Rating: (40) |
OK, So what measures should we take in order to use Webserver outside the local subnet (LAN)? Regards. Tomy.
|
Aim Higher |
|
3/30/2012 5:37 PM | |
Posts: 1 Rating: (0) |
Hi Ganes10, Would you be so kind to tell me how should I proceed to configure the PC so it can access the s71200? Im sure that Im working in the same subnet... but it is a fact that I have been able to connect with the s71200 from computers with TIA portal installed... I guess this must be becasue TIA portal adds the s71200 IP address to the PC so it can be recognized... How can I do it manually? Thanks in advance again! |
Follow us on