4/5/2012 9:25 AM | |
Joined: 8/30/2007 Last visit: 2/29/2024 Posts: 16 Rating: (0) |
I am using CPU1214C (firmware upgraded to V2.2) on TIA V11 SP2.Although I am able to download SCL blocks into the load memory(without MMC), the same is not possible using the MMC.Please confirm whether there is any Version of MMC to be checked for SCL compatibility ? Surprisingly, user program created without SCL blocks gets loaded into the MMC without errors & works in the PLC. The issue is only while loading SCL blocks onto the MMC. AttachmentS71200_PLC _SCL_Img.zip (301 Downloads) |
Follow us on